Other Parts Discussed in Thread: LM7480-Q1
Hi,
1. Is LM7481-Q1 recommended for use in 1000W+ applications?
2. Is LM7481-Q1 recommended for use in common source configuration (ex. similar to the reference circuits provided for LM7480-Q1 for unsuppressed load dump protection)?
3. If question 2 is YES, is it recommended for an array of multiple LM7481-Q1 in common source configuration be used for redundant power input with reverse voltage protection?