This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51397A: Mode pin function

Part Number: TPS51397A

Hi,

    From the spec, i know that the operation mode can be selected via mode pin.

But i am wondering if the operation mode can be dynamic change during operation.

i was also told that the device with above feature is being developed.

Could you help check it?

best wishes,

Jacky

  • Hi Jacky,

    For TPS51397A, the mode cannot be dynamic change during operation. The mode is fixed during operation.

    By the way, it's true some new devices are in development. Could you share some more detailed information of the requirements in your application? Does it have the requirement for the dynamic change between OOA and PSM mode? Or some other kinds of need for the dynamic mode change?

    Thank you very much.

    Andrew

  • Hi Andrew:

                For Arm platform laptop power design, it is necessary to have this feature to achieve lower power loss at S5 state and lower noise at S3 state.

                 The power rail is always on at both state. 

                 In additon, the converter VIN supply current(switching) must be less than 1mA.

    best wishes,

    Jacky

  • Hi Jacky,

    Thank you for the reply. I'm sorry that this feature isn't available in TPS51397A. But it's true that some devices are being developed.

    If you want some more information, you can send me email: andrew-xiong@ti.com.

    Thanks,

    Andrew