This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62866EVM-051: Efficiency test

Part Number: TPS62866EVM-051

Hi expert,

I test Efficiency of TPS62866EVM-051, find when load is 0.03A, the calculated result does not match the datasheet data. And Please see the attachment for my test data

Due to laboratory equipment, when the electronic load is set to zero, there will still be a load of 0.03A, and it is impossible to verify the efficiency of a smaller load. The current result of 0.05A and above calculated in the same environment is reasonable.

Could you please help to test the efficiency of the EVM board below 0.05A。
Thanks.
Best Regards,
Andy Liu │TI Analog FAE