What is the purpose of the OTG_RANGE_LOW bit? It seems that the possible range in the OTGVoltage Register is 0v-32.76v. In which case there is no need for the 1.28v offset or the switch to enable a lower range to target 3v. Also, with the 1.28v offset, and OTG min voltage of 3v can be defined whether the low range is set or not.
Am I missing something here? Also, is it fair to say that the strange almost powers of 2 in the datasheet OTGVoltage Register are typo's, and powers of 2 were intended? Or are those values from testing the chips?
Thank you,
Konstantin