Hi i want a dcdc converter with 3.7~4.2V input voltage to 40V output voltage dcdc converter which will be directly connected with load of 500 ohm.
1. Is it possible with tps55332 q1?
1-1. if not could you suggest the right converter?(or converters in series?)
1-2. It is available to conncet the tps55332-q1 in series to do so?
Thanks.