This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54232: 5V Output Design

Part Number: TPS54232


Dear Sir,

I am considering a circuit that uses a TPS54232 to generate 5V.

What is the reason for the "Choose R5 to be approximately 10 kΩ." listed in the data sheet (SLVS876D p15) ?

Since I want to choose from Standard Resistor Values (E12, E24), I plan to use the following.

Vout - R5 - VSENSE - R6 - GND
R5 : 4300Ω
R6 : 820Ω