This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5166: Variable output use case

Part Number: LM5166

Hello team,

I'm looking for a buck DCDC solution which can use with variable output use case and LM5166 would look to be a device.
Let me ask a couple of questions below.
1) Is the LM5166 able to be used with variable output on the FB resistors with Tr-SWs?
2) For example, I'd like to use 24V input pass through mode with 100% duty. Is there any limitation to use the pass through?
3) If 1) is possible, what should we care for the variable output range?

If you need more detail information, we can discuss further on the offline.

Thanks in advance.
S.Sawamoto