input voltage:20V
output voltage:13.2V
I think BQ25710 should operates in buck mode, but it works in buck-boost mode.
At the beginning, the input voltage is 5V, but when it up to 20V, the charger should change operation mode from buck-boost mode to buck mode.
Is there any way to adjust the operation mode?