This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1825B-SP: EOL tolerance on the current mirror that charges the CT capacitor spec

Part Number: UC1825B-SP
Other Parts Discussed in Thread: UC1825, UC1825-SP, UC1825A-SP

Hello,


My customer is trying to improve the tolerance on the internal clock on the UC1825B-SP, which is quite wide according to the spec sheet. It seems like the UC1825A-SP lists the tolerance on the oscillator discharge current. Is this the same value for the UC1825B-SP? Below is the commentary directly from the customer.

It would be very useful to know the EOL tolerance on the current mirror that charges the CT capacitor, which is not listed in the datasheet for the UC1825B-SP. We are considering adding an external current source to eliminate any tolerance associated with the 3V source applied to RT. Please let me know if you have any more information on UC1825B-SP clock.

Please let me know if any further information is needed.


Regards,

Joe