Dear all:
I try to configure data flash, but the DODaEOC Delta in Charge Terminaion and SOH Load I in data are not mentioned in the data sheet of bq27541. I don't know how to set..
Another, the current in my application is about 2A (normal), but the pulse current is about 15A(pulse width = 50ms), and the sense resistor is 10mohm, will the over-voltage of pin SRN/SRP cause the IC-bq27541 fail? Should I use the sense resistors 5mohm?
Who can help me?
Best regards
Jason