Hi, I need help !!!
I'm trying to use a BQ20Z60 based circuit (at the moment I'm working with an "equivalent" BQ20Z90 EVM circuit) to make a Gas Gauge (and Charge Termination) for a 8S NiMH Battery Pack. The batteries (AA, 2600mAh 1200mV nominal) are connected to the AFE as an equivalent 4 cells pack, with each "cell" made up by two NiMH cells. In this way, I obtain a cell nominal voltage of 2400mV, with COV threshold at 2860mV for a C/10 charging current at 25 degrees and a Timer of 10 hours maximum charging time and 40 degrees maximum Temperature.
I've made various trials to validate the Charge Termination method, and it seems to work quite good (at 25 degrees) ... I don't care very much if I terminate charging by Cell Overvoltage, Timer, Temperature or Overcharge alarm, without reaching a full charge situation.
The main problem I found is with the Chemistry ID for my NiMH batteries !!!!!!!!!!!!!! The Chemical Updater contains onli LiPo batteries or similar, and I'm afraid that the DOD(OCV,T) table is not good for the real OCV I'm working with ... for example, a fully charged LiPo has a 4200mV OCV, while my "cell" of two NiMH has a 2860mV OCV !!!
I know there are others Gauges (as BQ2060A) which works with NiMH, but I would like to use the BQ20Z60 for many reasons ...
Is it possible to develop a Chemistry file with a DOD(OVC,T) table for my topology ?????????????
What should I do ??????????
Thanks a lot,
Giovanni