Hello,
What is the maximum current value that can be passed through the TPS26600PWPT?
I made a board using TPS26600PWPT.
I accidentally shorted the device power supply in the circuit during the test, but the TPS26600PWPT did a good job as a fuse.
After that, I repaired the short circuit, but the FLT output of the TPS26600 started repeating Low and High.
I presume that the TPS265600 itself failed due to overcurrent.
Best regards.