Other Parts Discussed in Thread: TPS40210
Hi Experts,
Could you clarify if it is ok to externally load the BP pin?
In Datasheet it is stated that the voltage on this pin was tested within 0 mA < IBP < 15 mA.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
Could you clarify if it is ok to externally load the BP pin?
In Datasheet it is stated that the voltage on this pin was tested within 0 mA < IBP < 15 mA.
Hi Simon,
Yes, you can externally load the BP pin, but be careful to make sure thermal rating of device is observed. TPS40210 does not have thermal shutdown protection. Keep in mind also that when TPS40210 is disabled, BP regulator is disabled, so your load may lose its power source.
Thanks,
Richard