Other Parts Discussed in Thread: UCC21222,
Hello,
The Onboard charger requirement is 200V to 400V input, 48V output - 36A load.
Some basic details about main parts:
Full bridge transformer:
Primary inductance - 1025uH, Leakage inductance - 2.5uH
Full bridge MOSFET: IPW65R190CFDFKSA1, Coss - 86pF
Shim Inductor - 2uH
MOSFET Driver: UCC21222
Operating frequency: 230kHz
While the converter operating at above 300V DC input, at light load (3A) we observed failures in primary MOSFET due to over temperature.
We assume it could be because of the converter is not operating in ZVS mode due to resonance not met.
So now we are operating at 150V DC input and output voltage is set to 24V. We want to ensure ZVS before proceeding with the higher input voltage.
I have attached the test observation for your checking. The waveform includes voltage across primary and primary current.
In order to achieve resonance, we also tested with 330pF external capacitor connected across Drain and Source of Full bridge MOSFETs.
But we have not found better result.
We are continuing to tune the circuit to meet the resonance.
Please check the test observation and give your opinion about the waveform.
Also suggest us how to meet the resonance at light load conditions.
Please let us know if you require more details about the design or any other information.
It will be very helpful for us if you support.