This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25600: BQ25600-How to initialize charging parameters

Part Number: BQ25600


Hi team,

My customer is using BQ25600, their demand is  charging the battery to more than 90% battery power within 10 minutes, and the battery specification is 3.7v, 230mAh.

The question is if  bq25600 need ic initialization by MCU to charge the battery?

Thanks!

William

  • William,

    Referring to 8.3.1 Power-On-Reset (POR) and 8.3.5.1 Host Mode and Default Mode in bq25600 and bq25600D, after power-on-reset, the device starts in default mode with watchdog timer expired, or default mode. All the registers are in the default settings. The bq25600 is a host controlled charger, but it can operate in default mode without host management.

    Thanks,

    Ning.