Hello
in a new BMS board with bq40Z50-R2 and only 4 LEds I have an issue with BLINKMIDPT when in CHARGE.
Consider these settings:
BLINKMIDPT=ON
LED Hold Time = 4s
CHG Tresh1=0
CHG Tresh2=25
CHG Tresh3=50
CHG Tresh4=75
CHG Tresh5=100 (to keep it disable and avoid other LEDs to fluctuate due to charlieplexing)
If RSOC=33% when in Charge I have:
- LED1 = ON
- LED2 blinking fast at FLASH period (256 x 488us)
with the LED bar to stay ON for 4sec, then switch OFF for about 1sec, and then back ON again for another 4sec
If I remove BLINKMIDPT, setting the bit OFF, with same RSOC 33%, I have:
- LED1 = ON
- LED2 blinking normally at BLINK period (1024 x 488us)
with the LED bar to stay always on during the all the charge session
Why BLINKMIDPT is causing the LED bar to continuously switch off ?
Thanks in advance
Pietro