Hello Sir:
The SOH calculation method is FCC/Design capacity.
During the life cycle of the battery pack, will the calculation of the SOH value decrease from 100% to 0%.
Does the SOH value will jump or not during the life cycle process?
Example: cycle 1 is 100%, cycle 2 is 99%, cycle 3 is 98% and cycle 4 is 100%.
Is it possible happen? If it is possible can you provide us recommendations for us that how to let the SOH keep smooth and don't get back?
Thank you very much.