Other Parts Discussed in Thread: UCC28701
Hi team
Customer wants to enable/unable UCC28740. Do you recommend to use the circuit explained in below link?
Are there any good solutions else?

If you recommend this, please let me ask some questions about the circuit.
1. What is the resister value under Vdd? Is it 10kOhm? It seems to be 10N, but I am not sure what it is.
2. If VDD is less than VDD turnoff threshold, is it OK that UCC28740 is turned off and the Vout in the secondary side also goes to 0V?
Regards
Noriyuki Takahashi