This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1707: Dual MOSFET driver output latching high

Part Number: UC1707


We are seeing strange behavior of OUTPUT_A which should follow INPUT_A_NON_INV but latches high when the input is grounded.  Has anyone seen this type of latching behavior on the output?  Vc=Vin ~15V, OUTPUT_A remains high after INPUT_A_NON_INV drops.