Hi,
TPS2543 is of interest in CDP mode however there are a few questions if the response experienced is normal and way of implementing response needed for over current. Would like for the USB VBUS to cut off when there is an abnormal condition such as a short circuit.
Testing the TPS2543 on a power bank with a 700mA current limit shows that while the fault is tripped it continues to charge the device at 700mA with a 5V vbus. The question is, it possible to test the overcurrent limit with a device or would you need to create a short scenario as it seems like TPS2543 allows an overcurrent condition until it reaches a thermal fault, requiring the load to attempt to draw an excess amount not typically seen in compliant devices.
Please let me know what you think.
Best regards