This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5155: What is different between LM5155 and LM51551?

Part Number: LM5155

Hi,

What is different between LM5155 and LM51551?   Hiccup mode is only different, and both devices are pin-compatible.  Is it correct?  I want to confirm it.

Thanks and best regards,
M.HATTORI.

  • Hi Motoyasu-san,

    Yes, you are right that the LM5155 does not have the over current hiccup mode protection, but the LM51551 has it.  Please refer to the datasheet Section 9.3.10.   Other than that the two devices are basically the same and pin-to-pin compatible.

    Thanks,

    Youhao Xi, Applications Engineering