Dear,
Here my customer use TPS65132s for the bias supply of tablet LCD panel. We use the high-current application.
Vneg is set -5.7V, SYNC is high. We found the Vneg drop is about 425mV when there is a high current transient supply which is about 140mA~210mA considering ripple. So is this normal, do you have any suggestion to decline the Vneg drop to about 100mV? Thanks. And would you please help to verify on 65132sEVM what the actual Vneg drop value is when there is a 150mA current supply need. Thanks.