Hi team,
please help with the questions below.
1. Since it is a boost charger, what happens internally when VIN is greater than VBAT_SEC? Does it perform as a shunt regulator to provide a constant voltage?
2. if we use a Li-ion battery (3-4.2V) what would be the ideal solar panel voltage to connect to VIN?
3. Is it recomended to connect a 5V USB voltage to VIN in parallel to charge the battery since VBAT_SEC will always be much lower in voltage?
Thanks,
Kevin