This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Thermal Management

I am using this part in several locations to step down from 28 VDC.

Doing thermal calculations shows issues.I am showing a 108 Degree temperature rise from a 28 VIN to 12 VOUT at 0.41 Amps.

Is my calculations wrong?

LT3980
1st Stage
INPUT OUTPUT
V I TOTAL PWR EFF PWR V I
(vdc) (amps) (w) (w) (%) (w) (vdc) (amps)
28.00 0.22 6.21 3.00 0.80 2.40 12.00 0.20
3.21 0.80 2.57 12.00 0.21
6.21 TOTAL 4.97 0.41
PThermal °C/W TOTAL
4.97 45 223.65

Thans

David