Hi,
We have a customer with a concern as below.
I'm using LM317 for a 24 volt output. The input is at 35 volts. The load on the regulator is about 700 m.
1. what is the max operating temp of LM317 before the LM317 folds back and with this much heat dissipation.
2. is this beyond the limits of a TO-220 and should I consider a TO-3 instead?
Appreciate your help.
Roland