This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R3-DEVICE-FW: Upgrading Firmware - Learning Cycle, SREC, Configuration

Part Number: BQ40Z50-R3-DEVICE-FW

Hello! I'm looking to switch our bq40z50-R2 to bq40z50-R3. I want to better understand the implications for that.

Ok, so first I flash a new SREC (I downloaded the R3 firmware). At that point, what about:

1) My old configuration files (gg.csv). Can I still use these? Can I load them, and then re-export them to update the version? (Obviously there are additional settings I'll need to configure)

2) Do I need to reprogram the cell chemistry?

3) Does my old learning cycle still work? (loaded from the config file)

4) I assume I need to create a new srec file that includes the firmware, cell chemistry, and settings?

5) Do I need to do something in bqstudio, or will it know how to deal with the R3 version (so long as it's up to date)?

Thanks!