Customers now use bq24074 to produce rechargeable products. The battery charged is 5000mAh. The customer found that some batteries will not be recharged from 3.0V to 3.8V. At this time, the output of CHG (pin9) keeps jumping (output square wave), Iset (pin16) outputs low level, but it can be recharged from 3.8V to 4.3v after power failure. The circuit diagram is as follows, please help to analyze the cause? thank you.