Other Parts Discussed in Thread: TIDA-01606,
Dear all,
I am trying to create a system to test the gate driver cards E2 which are used on the TIDA-01606 power converter design.
I am having difficulties understanding how the DESAT function of the gate drivers ISO5852S works.
I would like to emulate a fault so that I can assess if the fault/reset function on the gate driver is working properly, however I do not understand what kind of signal I need to apply to the DESAT pin in order to trigger the fault. I have also read that the DESAT function can be configured to trigger the fault at some user defined conditions, however I do not know how to do this since I do not understand how the DESAT function works.
If anyone has any suggestions or can suggest any reference documents please let me know.
Thank you in advance.
Yours sincerely,
Adriano Arci