Other Parts Discussed in Thread: UCC256304
Dear TI,
I have an issue with an upgraded UCC256304 design. I've upgraded the design to the UCC256304 design accorfing to the excel calculator, the design seems to run well apart from the burst mode that doesn't run as expected.
To enable the burst mode I've done the following steps:
- I've chosen 'option 6' and selected Rbw_lower= 5.36k and Rbw_upper = 30k.
- Verified the in circuit resistance to be ~4554 Ohms
- Verified selection occurs (0.25V DC on BW pin) before start of the LLC waveforms (see waveform below)
- I've selected threshold of the LL/SS pin resistor values to be Rll/ss_upper = 137k and Rll/ss_lower = 56k which should yield a ~3.8V threshold according to calculation 70 and 71 in the datasheet.
My problem is that the device will not enter burst mode even when there isn't any load attached, I've further fiddled a bit with the design:
- I've fiddled with the values Rll/ss_upper and Rll/ss_lower get a higher burst threshold
- Used a resistor over the optocoupler to draw extra current from the controller and lower FBreplica
- Fed a small current to the secondary side output to offset, eventually causing it to shut down entirely without even reaching burst mode
It seems like no burst mode is selected although I think I've selected it correctly, could you please provide input on how to proceed next?