This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895: minimum input current

Part Number: BQ25895

Dear team,

The typical input current regulation range of BQ2595 is 100mA to 3250mA.

In the actual use scenario of the customer, the current is 10 to 20mA, can bq25895 still work?

Customer use solar panel, the current is very small when the light is weak.

Thanks.

Best Regards,

Qixiang Chen