This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC24624: can standby mode be disabled?

Expert 6760 points
Part Number: UCC24624


Dear Team,

we noticed the issue that the IC, in same load conditions, goes in standby mode and other times in normal mode, which causes an error on the output. Hence the question if the standby mode can be disabled? And what could cause this behavior?

Regards

Andreas

  • Hi Andress:

    the standby mode is designed for light load efficiency.

    The way to disable it is to let UCC24624 working without burst mode or with very low burst mode threshold.

    Please try to change burst mode or add fixed load on the output and try to see whether you can disable it.