Other Parts Discussed in Thread: TPS54418
Hello Team,
I have some question about RT/CLK pin. Could you please provide answer?
Q1. I want to use RT mode at power up. After that I want to change from RT to CLK mode. In this case, What is the recommendation circuit to switch the mode?
Q2. If the RT/CLK pin voltage pulled HIGH due to clock source failure, What behavior of the TPS57114C-Q1?
On the other hand If the RT/CLK pin voltage pulled LOW due to clock source failure, What behavior of the TPS57114C-Q1?
Q3. In CLK mode, we use 2MHz or 1.882MHz. In that case, Is there any constraint about RT clock frequency?
As I mentioned about Q1, I want to use RT mode at power up, then change to CLK mode. So I would like to know if there are any constraint about that.
Thanks,
Yuta Kurimoto