This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21520: what happened while DT PIN tied to 1/2 VCCI

Part Number: UCC21520

Hi support team 

What happened while DT PIN tied to 1/2 VCCI 

it's deadtime control or overlap behavior? 

  • Hi Red,

    To control the dead time, put a 500-Ω to 500-kΩ resistor (RDT) between DT and GND to adjust dead time according to: DT (in ns) = 10 x RDT (in kΩ). It is recommended to parallel a ceramic capacitor, 2.2 nF or above, close to the DT pin with RDT to achieve better noise immunity.

     DT tied to VCC will allow the outputs to overlap.

    We don't recommend operating or configuring this pin outside of these conditions.

    Regards,

    Krystian Plaskota