Part Number: UCC28740
Other Parts Discussed in Thread: UCC28600
Dears:
I would like to design a power by UCC28740 with one fixed transfomer, and 75V-140VDC input, output is adjustable between 10V - 110VDC, then drive a capacitive load by H-bridge.
An extra DAC connect to FB that help to set output change between 10V - 110V.
I did that adjustable output voltage design on buck/boost before, but I'm not sure it is still OK for flyback deisgn ot not. Is that design possible?