This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31520: about IHN pin.

Part Number: LMZ31520
Other Parts Discussed in Thread: LMZ31530

Hallo,experts,

 

In the LMZ31520 data sheet page 4 note (3), it is recommended to use a very low-leakage transistor to drive the INH pin (I<300nA).

Is it possible to relax the above leak current recommendation when the VIN voltage is high(12V , 5V,etc)?

 

I see functional block diagram on page 8 of the LMZ31530 data sheet.

The INH pin of the LMZ31530 is internally set by a resistor bridge between VIN (10KOhms pull-up) and GND (6.65KOhms Pull-down).

 

I think, the hi-level of INH pin is dependent of VIN value.

For example, if VIN=12V, the INH level will be 4.79V.

If VIN=5V, the INH level will be 2.00V.

If VIN=4.5V, the INH level will be 1.80V.

 

Even if the IHB pin is driven with a transistor leakage current of 10 μA, the voltage drop at the IHB terminal is 0.1 V (= 10 KOhms pull-up x 10 μA).

The voltage of the IHB pin considering the leakage current of 10 μA of the transistor is as follows.

If VIN=12V, the INH level will be 4.69V.

If VIN=5V, the INH level will be 1.90V.

If VIN=4.5V, the INH level will be 1.70V.

 

On the other hand,the high level threshold for INH pins is 1.8V.

 

When VIN is 12V or 5V, it exceeds the high level threshold of INH pin, so I think there is no problem.

 

Is it possible to relax the above leak current recommendation when the VIN voltage is high(12V , 5V,etc)?

 

Best regards

ATSU

  • Hi,

    Yes, it's okay to use a higher leakage current transistor (which may be the PGOOD of another regulator). So long as the voltage at the INH pin is above 1.8V, the LMZ31520 will be enabled.

    Regards,
    Kris

  • Hello, Kirk ,

    Thank you for your support.

    Sorry for the late reply.

    I appresiate your answer.

     

    Let me ask you another question about the INH pin.

    Is it possible to add an external pull-up resistor between the INH pin and VIN?

     

    If VIN = 4.5V, the IHN level is 1.80V when the INB pin is open.

    This level is close to the high level threshold of the INH pin.

    I want to add an external pull-up resistor between the INH pin and the VIN.

    For example, if an external pull-up resistor of 10 KOhms is added, the IHN level when the INB pin is open is 2.57 V [= 4.5 V * (6.65 KOhms / (6.65 KOhms + (10 KOhms // 10 KOrms))].

    Is it possible to add an external pull-up resistor?

     

    Best regards
    Atsu

  • Hi,

    Yes, it would be fine to add an external pull-up, but make sure that over your full input range that the INH voltage does not exceed 6.5V (abs max 7V).

    Regards,
    Kris

  • Hello, Kris ,

    Thank you very much for your reply.
    My question has been resolved.

    Best regards
    Atsu