Hello,
as far as I can tell from the datasheet, the TPS26633 and the TPS26636 are identical, at least in the HTSSOP variant. Is there a difference I am missing?
Best regards
Felix
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Felix,
The difference is in the Overvoltage clamp level.
TPS26633 clamps to fixed 35V where as TPS26636 clamps to fixed 39V. It needs to be updated in the datasheet. I will take action in the next datasheet revision.
Best Regards, Rakesh
Dear Rakesh,
thank you for your answer.
In that case, what is the difference between the TPS26635 and the TPS26636 then? Is it just the package options?
It's a bit confusing, because the -3 is available in both VQFN and HTSSOP, while the -5 is VQFN only, and the -6 is HTSSOP only.
Thank you & best regards
Felix