Hello expert,
My customer has a Boost application, condition as below. They would like to use TPS61288 for this application. But input peak current might be reach 15A current limit if we use 90% for efficiency with minimum input voltage. May I know if you can help to double check the output power and suitable suggestion on this case? Thanks a lot!!
Condition:
Vin=3.4V~4.2V
Vout=7.4V
Iout=peak 6A, nominal 3A~4A
Best regards,
Ann Lien