Other Parts Discussed in Thread: TPS552882, TPS55288
Dear TI technical support
Presently i try a TPS55288-EVM045 board. This buck/boost works very well for my application. But i need the GUI interface to configure each time the output voltage at 12V and activate the output to use it. Do i need absolutely an external I2C controller to use the evaluation board for an application ?
I have an application and i need to develop a 15 power supply units
Specification (3-36V input, Output 10V or 12V at 2A) for a project. Is there a possibility to produce 15 evaluation board of this type with a special programmation to have to the good output parameters and the output enabled all the time by default ?
How can i use your product simply ?
Do I need to produce a circuit with the WEBENCH Design tool ?
It’s probably more expensive and I don’t know if an external i2c is required.
Thank for you support
Yannick Bouchard