Other Parts Discussed in Thread: TPS27S100, TPS1H100-Q1
Dear Forum Members,
I am planning to use the TPS22810 load switch to switch a 12 V rail that supplies approx. 3 A. I would like to connect multiple TPS22810 switches in parallel to share current and lower the power dissipation in the switches.
Can these load switches connected in parallel? If so, are there any precautions to take or is it as simple as just paralleling them? The document "Parallel Load Switches for Higher Output Current & Reduced ON-Resistance Design Guide" suggests that it is, but I'd like to make sure that what the document shows is also applicable to the TPS22810.
Thanks and regards
Daniel Nagy