This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5046: Do you have a application note ?

Part Number: LM5046
Other Parts Discussed in Thread: UCC28951

I'm going to design as below by LM5046.

Vin:380V(PFC Voltage)

W: 500W

Do you have a similar application note , send it to me.

  • Hello,

    For high voltage applications we recommend using the UCC28951 instead of the LM5046.

    We have a 600W EVM you can evaluate if you wish.  You can find the user's guide at the following link.  

    The following link will bring you to an application note that gives a design example based on the 600W EVM.  I think your customer will find this useful.

    If your customer is interested in using the UCC28951 and has questions in regards to it's operation.  Could you repost with UCC28951 in the title of the thread so the appropriate applications engineer can provide support?

    Regards,