Hi everyone,
just a small question about the TPS1088 boost converter. I'm not sure what the threshold is for the EN (enable) pin. I see that it has a max rating of -0.4 to 7V, but not sure what the threshold between logic 1 and 0 is.
I plan to use an 18650 battery, so I would connect the enable pin to the battery (hence the enable pin would receive 4.2 to 3.3V).
Any help would be much appreciated!