The datasheet claims on Pg.1, the below two as far as startup timing is concerned.
"Adjustable input settling time (SS)"
"Adjustable output soft start time (SS)"
I have achieved the slew rate I need with a 56nF SS cap. The question is, without affecting this, how do I reduce the Input settling time?