My customer needs to generate a negative and a positive Voltage that they plan to generate using two DCDC (or alternatively one DCDC generating both voltages)
Condition: The max height on the PCB is 5mm, which is likely a problem for the capacitor and coil. Please keep this in mind when proposing the two DCDC.
Vin = 24V / +/- 10%,
Vout1 = -5V to -6V with 0.3A
Vout2 = +6V with 0.3A to 0.4A
What can we propose?.
Thanks
Josef