Part Number: TPS61500
Note i can supply direct to a TI app engineer by email ----- specific pdfs of the 2 schematics when requested but will not post them on a public ti portal
Number: CS0315134 Contact: cd feak First name: cd Last name: feak Short description: not seeing drive capability with my design Phone: 16266428886 Email: cdfeak@psadvancedeng.com Company: azure medical technologies Company phone: Language: English State: Open Provide case details or comments: hi richard i am a bit stuck here
changed my design to 9 of the cree xpred 701 series 630nm parts from the original 5 of those parts.
www.mouser.com/.../XLampXPE-221789.pdf
was able to make the 5 series cree work just fine with 400mA as drive...and up to 7 of the same parts
now just cannot get the part to power 9 of these at anywhere near their rated optical output even with I drive set for 400mA----they are just real dimmed down with 9 of them series hooked now.
ATTACHED ARE THE ARRAY AND THE DRIVER PCBA SCHEMATICS
lipoly 3.7-4-2vdc 2400mA 1 c rive capability (its not the battery---i also directly hooked a dc 4v power supply thinking first maybe battery was straining to meet the 1A ---even though 400 is way below that 1A)
what might be wrong here?
have a good sumida inductor and a low dcr 3a schottkey
supposed to be a 40v switch --- the crees vF totals are not adding to 40v
operating no pwm---steady state=== yes a higher load on output but it seemed this part should handle ok
CD (Don) Feak
Azure
AMT Global (Calif C- Corp)
Technologist
626-642-8886 Office
626-281-9531 Fax
WhatsApp: c feak
WeChat : cdf62xke
SMS/Mobile +1 626 841 4856
LINE: cdfeak or cdfeakusa
Skype: cd feak or roadster62xke
cdfeak@azuremedtech.com
www.azuremedtech.com
On 3/22/2018 7:06 AM, support@ti.com wrote:
>
> Don,
>
> I am sorry that I could not call yesterday, but I have no company phone at my house.
>
> Please let me know if you have any further questions or comments.
>
> Regards,
>
>
>
> Richard Elmquist
> TI Applications Support
> Americas Customer Support Center
> 512-434-1560
>
>
>
> http://e2e.ti.com/
>