This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3809: Abnormal behavior at startup

Part Number: TPS3809

Hi team,

My customer found below behavior of TPS3809K33, as you can see at the startup, well after 3.3V VDD is established, the reset output stayed at 1.1V for about 200ms, then goes up to 3.3V. 

This seems not the normal behavior of this device according to the timing diagram. What do you think? 

Thanks

George

  • Hi George,

    Can you share a schematic?  Is the result from an EVM board?  From a customer's system?  

    Yes, the output does not look correct.  The output looks like it is being pulled up when it should be low.  

    Ben