Can this chip be used in the situation that the frequnency is very low? For example, this chip should control the high side mosfet and the low side mosfet both being ON for more than 60 seconds. At this period, these mosfets won't be turned off. In this situation, can the bootstrap capacitor provide enough energy on VDD without charging?