This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: Application guide how to configure automatic learning procedure and EOS feature

Part Number: BQ34110

Dear support team,

we are using BQ34110 IC at our custom design of the UPS system, to check battery status and battery health.

According to TI post (How do you detect battery aging in rarely discharged applications) - it is possible to discharge the battery by 1%-2% to check EOS.

Questions:

  1. Do you have some application notes, how to configure gauge IC for automatic learning procedure, that should run periodically? 
  2. Will the gauge provide accurate information about battery charge In case if learning procedure will run periodically with discharging by 1% -  2 %? Or at some point, full discharge is needed?

--

Best regards,

Sergii Makovetskyi