This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS4H000-Q1: Current limit

Part Number: TPS4H000-Q1

Hi Experts:

A few questions about TPS4H000-Q1 to check with you:

1. The current limit value set by CL pin is the current limitation for each channel, not the total current for 4 channels, right?

2. The max norminal dc load current in datasheet is 0.75A, why the internal current limit value can be 1-1.6A?

3.  What's the minimum current limit value customer can set? Is there any limitation here? My understanding is that as long as the accuracy can meet the requirement, customer can set the current limit value as low as they like, right?

  • Hi Arie, 

    Arie Li said:

    1. The current limit value set by CL pin is the current limitation for each channel, not the total current for 4 channels, right?

    Correct. 

    Arie Li said:

    2. The max norminal dc load current in datasheet is 0.75A, why the internal current limit value can be 1-1.6A?

    This is difference between a transient and dc condition. its more about heat and protection of fet why the DC condition doesn't equal internl Ilim. 

    Generally you may not always want to have a hair trigger current limit, and even external current limit > DC condition. A relatively small dip above a stable dc current wont kill the device but a true soft or hard short to gnd will because that will become the DC condition or current will rise until IC buries itself.

    Regarding the internal vs ext current limit, please see here for an E2E from one of my colleagues supporting these de ices. 

    FOr #3, what You've said is basically correct but i will loop in my colleague who supports this product family who can better answer this question with more authority.

    I am marking thread as closed for now and ping my colleague, please wait for reply. 

    Best

    Dimitri

  • Hi Dimitri,

    Thank you for your help. Expect the reply from your colleague by today. It seems the link you shared is lost, I cannot open it.

  • I am sorry but have got no reply, we have some of the team out of office so are stretch thin let me ask again.

  • H Arie, 

    Current limit is characterized down to 50mA so that is the minimum recommened. 

    Best

    Dimitri