Part Number: TPS62135
Hi,
We can't find the efficiency curve for the case of VIN=5V/VOUT=1V. Can we have the efficiency number under such scenario when Iload is 0A/1A/2A/3A/4A respectively?
In parallel, we're using these chips for two cases as below. Please help us to judge if the undershoot value is reasonable or not.
- Case1: VIN=3.3V/VOUT=1.2V
- Case2: VIN=5V/VOUT=1V
Thanks,
Antony