Hi Team,
I have some question about LP8867-Q1 EVM Board (SNVU648) as below:
1. Does the function of FB2 (220ohm) & C17,C18,C19,C20(2200 pF) filter the harmonic of sw frequence 400K HZ??
or has other function??
2. For EVB board design, it use net to connect AGND & PGND,
Can it use 0 ohm resistor to connect AGND & PGND??
Or can only use single GND , not to divide AGND & PGND??
Thanks.